Industry Online Support
Technical Forum
12/7/2021 9:20 AM | |
Joined: 2/15/2021 Last visit: 12/11/2023 Posts: 16 Rating: (0) |
Hey programmers. Im having a strange issue with my logo's running LWE in the cloud. i have 4 logo's running different programs ( in the same environment ) but over time, normally 3-4 days they loose connection through the cloud. ( all values become 0 ) The problem is not happening at the same time / specific time, its seems completely random. To solve the problem i open LWE and upload the (same) program to aws, and then i have connection again for the next 3-4 days and so on... When i have no connection thourgh cloud i can still see values in things ( device shadows ) I am 100 % sure the logo controllers has not been powered off or disconnected from the internet. i have attached pics of the AWS,shadow, LWE environment. Anybody experienced something like this, or might have a solution / idea ? AttachmentScreenshots.zip (265 Downloads) |
Last edited by: Jen_Moderator at: 12/07/2021 11:50:15Added all files as a zip file. |
|
Follow us on