4/15/2024 11:06 AM | |
Joined: 12/18/2014 Last visit: 7/3/2024 Posts: 33282 Rating:
|
Can you upload your LWE project and your LOGO! program as a ZIP file? |
4/15/2024 11:12 AM | |
Joined: 5/30/2022 Last visit: 7/2/2024 Posts: 542 Rating:
|
Hi TwistedTeknician, What version of Logo do you have? If you have a V8.3 I would recommend restoring it with the following tool: Reset Tool for resetting LOGO! 8.3 to the delivery state After that, try to download the project again. |
If this information really helps, you could use the Rate function. |
|
4/15/2024 11:15 AM | |
Joined: 12/18/2014 Last visit: 7/3/2024 Posts: 33282 Rating:
|
What has the reset of the base module to do with the loading a of page of the webserver? |
4/15/2024 12:33 PM | |
Joined: 7/1/2023 Last visit: 5/15/2024 Posts: 67 Rating:
|
Hi folks I think I have found the issue - it seems the SD card was defective in some way. I formatted it a few times and still no luck so I replaced it with a spare and all good. Cheers |
This contribution was helpful to
2 thankful Users |
4/18/2024 4:53 AM | |
Joined: 9/11/2014 Last visit: 7/3/2024 Posts: 729 Rating:
|
Please note: If you change a LWE project and you download to LOGO!, then you also have to "load" it to the web browser. Simplest way is to press F5 in the browser. Then the browser will load all data from the web server once more and display the changes. Hope this helps |
Follow us on