5/12/2015 11:41 AM | |
Posts: 10 Rating: (0) |
Thanks for fast answer ! |
5/12/2015 1:30 PM | |
Posts: 1299 Rating: (135)
|
Hello, on the event "loaded" of the screen you can call the system function "SimulateTag". With this system function a tag will be simulated in a defined cycle (multiple of 200ms). With your scenario I would use the cycle 50 and call the screen change on the event value changed of this tag. https://support.industry.siemens.com/cs/ww/en/view/109091876/56856939915
K!ke |
5/12/2015 4:02 PM | |
Joined: 10/21/2013 Last visit: 7/27/2023 Posts: 416 Rating: (28) |
Hi kike, thank u so much it is great.. i have attached doing in hmi tp1200 v13sp1 someone can find it helpful... AttachmentSCREEN CHANGE.zip (125 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on