10/6/2020 6:42 PM | |
Posts: 16 Rating:
|
Hi All! Thank you for your time. Here is my problem… ill try to give a good context of information, please ask for more if needed. There is an electrical panel with two ABB drivers and an IM153. Everything on profibus. Three months ago i changed the program who work with all these signals. After two months and a half working without problems, all blocks connected to these elements went to Maintenance State (red maintenance symbol on blockIcon, Signal BAD = 1, Mode <> 16#80, MS <> 0). Is suspected that the electrical panel have lost power before this problem appears. Almost all the program work without Module Drivers diagnosis on this PLC. Temporal solution: I cannot find what is happening. See in attached images things i checked.º Here an explanation of each image attached: ABB dp diag OK: hardware diagnostic of a driver without problems connected to that profibus ET200 diag int: hardware diagnostic of the IM153 with MS problems Find in my google drive all the images: [snip] Please help! ...and again, thank you for your time. Federico AttachmentMS Problem-20201007T074347Z-001.zip (73 Downloads) |
Last edited by: Fedena2507 at: 10/06/2020 18:45:58Last edited by: Jen_Moderator at: 10/07/2020 09:45:50Removed link and added file as an attachment. |
|
Follow us on