9/21/2023 12:47 PM | |
Joined: 9/7/2023 Last visit: 5/16/2024 Posts: 5 Rating:
|
Hi everyone, I have made the topic https://support.industry.siemens.com/forum/be/en/posts/control-2-solenoid-valves-with-3-pushbuttons/305012/?page=0&pageSize=10 before. I have changed the setup I want to achieve a little bit. Let me explain what I want to achieve: * I have two solenoid valves to control, with a light indicator after each valve to check valve state (4 outputs) * I want to have a timer to open/close the valves automatically (open from 02:00 to 18:00, closed the rest of the day) * I want a switch to change from timer to manual open/close (each valve would be controlled by a momentary pushbutton) * When between 02:00 and 18:00 when I change from manual to automatic, both valves should go open * When between 18:00 and 02:00 when I change from manual to automatic, both valves should close My problem I can only get one of these to work. When I change my FBD either the automatic on works within working hours, but not automatic off outside the hours or vice versa. I have added my FBD as PDF because I can't upload LSC files. Could someone please help me in the right direction? Thanks in advance AttachmentProbeersel.zip (337 Downloads) |
Last edited by: PLC_tryout at: 09/21/2023 13:19:16 |
|
9/21/2023 1:19 PM | |
Joined: 9/7/2023 Last visit: 5/16/2024 Posts: 5 Rating:
|
I have added the LSC as ZIP as suggested |
9/21/2023 5:31 PM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33344 Rating:
|
Try this.
AttachmentProbeersel_V2_0BA5.Standard.zip (391 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on