9/30/2019 8:11 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
You have an active operative blocking - permission to be no control, yet releases the lock. |
9/30/2019 8:11 AM | |
Posts: 2 Rating: (0) |
Dear Jay, in manual mode, these buttons are enabled for other motors . there is a setting to enable/disable this button. Actually, i need this setting. |
9/30/2019 8:18 AM | |
Posts: 1283 Rating: (105) |
if you have thew project file, you might be able to go in offline mode and see what setting had been made to that On/OFF graphic buttons or faceplates. |
9/30/2019 1:02 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello 12345678554, can you send a screenshot from the CFC with the motor block? with regards |
Follow us on