Industry Online Support
Technical Forum
11/24/2009 8:40 AM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating:
|
Hi Poo.., poor man if you are using SOAP Could this help you: http://support.automation.siemens.com/WW/view/en/39099329 this uses the real WinCCflexible internal Web-Server ("MiniWeb") with real HTTP-protocol. Ok to your question. 1. I guess you are using the original Startup-Code for the SOAP-option?! 2. From where do you try to access your CentralStation with activated SOAP-option? same PC / internal private networ / external internet 3. Do you use the simple-option or the complexe one? 4. Did you try to restart the MiniWeb by right-clicking on it.... 5. Can you "ping" your names which you entered in the "hosts"-file regards |
Follow us on