2/24/2009 2:31 PM | |
Posts: 20 Rating: (0) |
Hey now i also call sms receive and now different, i cant make a good sms_init at the site where i can be online to see what happens it stops on status word 2 echo off found out that i have version 2.0 of the library and that one works good also with my setup, SM_INIT is done in a couple of seconds and also SMS_SEND still i cant understand how to use SINAUT MICRO SC S7-200 Block Library Update V1.16 to send SMS with my TC 65, is that possible? what i have done in my project: 1. used version set5_s7-200-library.mwl version 1.15 worked to send sms, but some time SMS_INIT doesnt work, 2. deleted every POU in my project that is for SMS handle, installed set5_s7-200-library_port0.mwl Version 2.1 and now SMS_INIT doesnt work, now what i think to try to night, deleted every POU in my project that is for SMS handle, in library memory allocation im going to delete library symbols setting up new calls for sms_init,send, receive with version 2.0 in my project, and hope it works. next step is to increase waiting time in block sms_xmt_rcv_manage so it have longer time to login to the GSM network i was told that is in network 10. Attachmentsmstest_V2.1lib.zip (131 Downloads) |
2/24/2009 3:36 PM | |
Posts: 20 Rating: (0) |
When i make a version check with 2.0 it seams to go to make a update but a version check with 2.1 it doesn't looks so i have attached 2 print screens haven't done any update yet, going to try it to night.. Attachmentversioncheck.zip (120 Downloads) |
3/11/2009 9:58 PM | |
Posts: 20 Rating: (0) |
Connected with HyperTerminal to the modem with 9600 speed sending this AT commands: AT+CPIN?$R +CPIN: READY AT+IPR=9600$R ERROR AT+IPR=9600 ERROR ATE0$R ERROR
AttachmentSMS_lib2.0_sms_check.zip (148 Downloads) |
3/11/2009 10:09 PM | |
Posts: 20 Rating: (0) |
Was unpluging the ppi cable and now i got TX/RX flashing, but still no sucess SMS_INIT |
Follow us on