6/24/2010 10:25 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello engyasso; If you are following the MAS 21 documents, you should have already most of your qnswers already: http://support.automation.siemens.com/GB/view/en/27038105 Besides the setup and code documentation, there is a sample program available there to guide you in using the various function blocks used in the application. The basic physical requirements for this application to work (as it is proposed by Siemens) are copied here: MPI cable 1 6ES7901-0BF00-0AA0 RS232C cable 1 6NH7701-5AN 1:1 Cable (no Null-modem Cable) SINAUT ANT 794-4MR 1 6NH9860-1AA00 GSM Quadband and UMTS SIM card 1 Available at your mobile services provider.(Often special M2M are available for GPRS) MMC card 1 6ES7953-8LF20-0AA0 Min. 64kByte DSL Router+Modem 1 Specialist dealer with port forwarding Fixed IP address for DSL (broadband) connection 1 Can be ordered at your provider You must determine whether what you are providing matches the minimum requirements for the application. If not, it would be advisable that you modify your setup to match the requirements. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/24/2010 10:52 PMLast edited by: dchartier at: 6/24/2010 10:27 PM |
|
Follow us on