Industry Online Support
Technical Forum
5/12/2010 10:53 AM | |
Joined: 5/28/2008 Last visit: 7/15/2024 Posts: 1343 Rating: (141) |
Hi, try to reset modem by pressing Reset Button for more then 5 seconds. Then we'll see.. |
5/12/2010 3:43 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24)
|
Hi, check your m2mopc.log-file in C:\program files\siemens\sinaut micro sc\. maybe there is an indication whats going wrong. Please refer to http://support.automation.siemens.com/WW/view/en/23117745 Regarding the LED´s behavior everything is fine till the Modem log into the Providers GPRS Network. But it´s not able to connect to the server. Did the customer make any changes on Central Station side? regards Lif |
Follow us on