11/11/2016 2:42 PM | |
Posts: 9 Rating:
|
Hello, I wrote a plc program; Master-Slave DP System without using DP/DP Coupler. It is working very well. However ı want to add the drive ( CU 240 E and 1,5 kW Power Module ). Hardware configuration is okey. No problem. 2 CPU's RUN green light is ON and at drive RDY light is green. I added the drive on master plc profibus system. Because ı can not add the drive on slave plc profibus system. So ı want to control drive with slave plc by using master PLC Profibus Network. How can ı do that? Or Can I transfer the data to the drive with using DIRECTION is from Slave to Master ? My plc program is attached. Kind Regards, Musa UÇAN AttachmentCpu__and.zip (61 Downloads) |
Follow us on