Industry Online Support
Technical Forum
1/7/2010 12:43 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating:
|
Hello, have I understood correct that you have two S7-200 station with EM277?? One station works as DP master and one works as DP slave??? In the following manual "S7-200 System Manual", chapter "Appendies -> EM 277 PROFIBUS-DP Module Specifications", you can find more information about the DP master and DP slave functionality and configurationof the S7-200 station with EM277. http://support.automation.siemens.com/WW/view/en/1109582 Or look at here (chapter 4 "PROFIBUS"). http://support.automation.siemens.com/WW/view/en/25074283 Good Luck Little Holmes |
Follow us on