12/13/2009 4:28 PM | |
Posts: 40 Rating: (1) |
thanks you for your reply. |
12/14/2009 12:54 PM | |
Joined: 9/27/2006 Last visit: 10/20/2024 Posts: 12290 Rating: (2688) |
Hello Berno; I cannot locate the manual, but maybe the following posting from diwa can contribute: /tf/WW/en/Posts/17883 Hope this helps, Daniel Chartier |
12/14/2009 1:42 PM | |
Joined: 6/4/2008 Last visit: 10/10/2024 Posts: 1502 Rating: (324) |
Hi, here is my copy of the testbox manual, it is scanned, so a bit crappy!! To be honest, I use Diwa's descriptions as per the previous link, I think you will agree, they are far simpler than what the manual contains. Note, the testbox is useful, but don't rely on just this. I have had the transistors all showing healthy with the testbox at 24VDC, but breaking down under load conditions. Cheers, Graeme
AttachmentTestbox.pdf (780 Downloads) |
Last edited by: Graeme at: 12/14/2009 1:45 PM |
|
Follow us on