2/1/2017 3:58 PM | |
Posts: 14 Rating:
|
Dear Experts, I have a problem with one Siemens Masterdrives 6SE7018-0EP50, that is connected to motor 1FK60603-6AF71, on a vertical spindle drive. In attachment I'm sending drive parameters that are downloaded from drive via DriveMonitor. The problem is this: When the motor is connected to a spindle, and after I give it command to run, it doesn't move. It has two speeds, and direction control with joystick. On both speeds it wont go. After this, I removed the motor from spindle, so it is now free from load. When I give command for 1.st. speed, the motor moves, but gives some strange sound, and doesn't run at constant speed, it accelerates and deccelerates constantly. In 2.nd. speed it runs ok, the display on the drive shows 250. Can anybody help me with my problem, what could be the reason for this? Thank you in advance AttachmentBrekston3_2.zip (268 Downloads) |
Follow us on