Industry Online Support
Technical Forum
7/14/2013 2:57 PM | |
Joined: 8/25/2006 Last visit: 6/26/2024 Posts: 2207 Rating: (278) |
Hello. Which type of connection you mean? GDM, CP5100 or CP51M1? For communication via IE max. telegram lengths: CP5100 - 64kbyte (send), 55 kbyte (receive) CP51M1 - TCP/IP - 32kbyte, UDP - 2kbyte For more information on perfomance look at themanual,chapter 3.5.4.4 and 3.6.4.4. For GDM coupling I could not find any limitation in the manuals and I think all is limited by CP52M0 memory, which is 2Mbyte capacity. For perfomance of GDM coupling look in the same manual, chapter 3.3.5.
|
This contribution was helpful to3 thankful Users |
Follow us on