7/22/2019 2:41 PM | |
Joined: 5/6/2010 Last visit: 4/28/2024 Posts: 1965 Rating: (272)
|
Hello, at teh atachment you can find a example for IO-Device-communication. This example contains the following
Please look at this project in TA V15.1. If you have any questions... regards AttachmentTest_IO_Dev.zip (238 Downloads) |
This contribution was helpful to2 thankful Users |
7/22/2019 2:56 PM | |
Posts: 111 Rating: (29) |
@CaOd: My suggestion would have been to use Open User Communication (Ethernet TCP). https://support.industry.siemens.com/cs/ww/en/view/109747710
|
Last edited by: AutoGen_1801304 at: 07/22/2019 14:58:33 |
|
7/22/2019 3:07 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349) |
TIA Portal automatically calculates the update rates for the i-Device's. If that becomes unacceptable to the OP, other means of data gathering will be required to meet the update rate requirements.
|
science guy |
|
7/23/2019 8:00 AM | |
Joined: 5/6/2010 Last visit: 4/28/2024 Posts: 1965 Rating: (272)
|
Hello, huggy_d1 mean's that you can use the 1200er as a "normal" PLC with a own PLC-programm. At the attachment you can see a V14-project with the same configuration. Your consideration about hte maximum I-Device's.. the 1500 have a I/O-area of 32k = 32768 Byte. If you have any questions... regards AttachmentTest_I_Device_V14.zip (145 Downloads) |
Follow us on