3/26/2018 5:17 PM | |
Joined: 9/27/2006 Last visit: 1/13/2025 Posts: 12325 Rating: (2697) |
Hello mohammed; From the information you are providing it is difficult to provide help with any degree of certainty. Have a look at the maintenance manual for the Maxum II system: https://support.industry.siemens.com/cs/ww/en/view/109480740 The screenshot below shows corrective actions to be taken with different status combinations of the PECM LEDs. This could be a starting point for your intervention. You will also find installation, replacement and wiring diagrams that can help you out. If you receive alarms on the controller, there are also tables in the manual showing corrective actions to be taken when each one appears. Unfortunately quite a few interventions point to "Contact Customer support"; in that case I can only suggest you contact the vendor who sold you and installed this analyser system and require his presence on-site. Hope this helps, Daniel Chartier |
Follow us on