3/22/2022 9:21 AM | |
Joined: 8/3/2009 Last visit: 9/13/2024 Posts: 13672 Rating: (1725) |
Hello fabioga66 perhaps on of these links can help further: https://support.industry.siemens.com/cs/ww/en/view/109772940/89566547339 Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/25/2023 7:46 AM | |
Joined: 8/28/2018 Last visit: 5/22/2023 Posts: 1 Rating: (0) |
Hello Fabio, Edit: Modbus TCP is used and the PLCs are interconnected directly from X1P2 to X1P2 without any additional hardware since it´s just a test prior to deploying it at the facility. In the test code 5 words shall be read from the server and 5 words transmitted to the server. Edit2: As promised attached you can find the report / description. Best regards, AttachmentModbusTCP_Report.pdf (345 Downloads) |
Last edited by: FVZ_ekb at: 04/25/2023 08:03:33Last edited by: FVZ_ekb at: 04/27/2023 16:00:15 |
|
This contribution was helpful to4 thankful Users |
Follow us on