4/2/2024 3:08 PM | |
Joined: 4/2/2024 Last visit: 4/16/2024 Posts: 2 Rating: (0) |
Hi, it's my first post here and I have a subject in university about industrial network and my teacher is really bad and can't help my group with why the error is happening or how to do it the right way . I'm using the TIA Portal v14 and Logo V8. The Logo! ip: 192.168.0.30, the S7 ip: 192.168.0.50 and my network adapter's ip: 192.168.0.1. Every component have a default gateway as 0.0.0.0 and subnet as 255.255.255.0. I can send my program to both S7 and Logo! but when I start to monitoring the the S7 my MB_CLIENT block shows an error with the status:16#80A4. I already searched for what that status flag means and says that the local IP is the same as the remote IP but I configured everything with different IPs and the error makes no sense to me. Even changed my switch to another, change cables, tried to make the S7 server and Logo! client but still no response. I'm sending a link to an OneDrive folder: Industrial_Network (I don't know if it's against the rules of this forum but I'm really desperate) If anyone could help me how to solve the problem and guide me to how to do correctly I would be very grateful. AttachmentIndustrial_Network.zip (16 Downloads) |
Last edited by: Jen_Moderator at: 04/03/2024 08:07:11Link removed and file attached. |
|
Follow us on