9/8/2016 10:23 AM | |
Joined: 6/16/2015 Last visit: 6/13/2024 Posts: 21 Rating:
|
Hi According to intruction We need to do an exception for hh_wincc.exe file when enableing application contorl on PCS7 Servers and Clients I used sadmin attr add -a "c:\program files (x86)\siemens\wincc\bin\hh_wincc.exe" for the exception. But in eventlog application control still says it prevented hh_wincc.exe to be modified. I have double checked and this file are solidfied. Mcafee documentation are not so clear here. Do you have any experieced of this? Maybe Iam useing the wrong flag? I am useing stand alone mode for Application control and running PCS7 V 8.1 SP1 and Mcafee Application Control 6.1.3 , they should be supported accorting to the supported Software list. Thanks in advance |
Last edited by: Mats_J at: 9/8/2016 10:31:12 AMLast edited by: Min_Moderator at: 9/8/2016 3:24:48 PMEdit link to permanent one Last edited by: Mats_J at: 9/9/2016 11:29:01 AM |
|
9/26/2016 10:52 AM | |
Posts: 567 Rating:
|
Hi, did you solve the problem? Maybe you should not write the hole path the the file "hh_wincc.exe". Maybe sadmin attr add -a hh_wincc.exe is enough. |
Follow us on