6/23/2011 2:08 PM | |
Joined: 5/19/2011 Last visit: 12/23/2024 Posts: 196 Rating:
|
Dear All I have 840C MCP type no is-6FC5703-0AD03-0AA0.The MCP is not giving any response means jog or other keys are not working,The input for respective key is also not coming.I hhave checked that 5V is coming in pin 34 & 52. only MDA & feed hold, cycle stop LED's are glowing. Please help me.. Splitted from 840C no response from Keyboard Panel. |
Last edited by: O_Moderator at: 6/24/2011 9:22 AMnew subject after splitting |
|
6/24/2011 9:23 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread 840C MCP. Best regards O_Moderator |
Follow us on