11/18/2010 9:27 PM | |
Joined: 9/27/2006 Last visit: 5/16/2024 Posts: 12257 Rating: (2668) |
Hello Moonbeam; If your program was built based on the use of this positionning software and your present computer does not have the software package installed (and properly licensed) you will not be able to open the dedicated functions created for the application on this new computer. I would suggest you contact the person(s) who developped the project and ask them for the required licenses.Since this softwarehas beendiscontinued for at least 5 years, you might have trouble locating it through official Siemens channels. Here is some information I was able to retrieve on the subject: Manual for MCU-PIT (SIMODRIVE 611Single-Axis Positioning Control MCU 172A) http://support.automation.siemens.com/WW/view/en/22073867 MCU is the abbreviation for Motion Control Unit. PIT stands for Parameterizing and Commissioning Tool. In other words, the MCU-PIT software package can be used for the complete parameterizing and commissioning of the single-axis positioning control MCU 172A. Scope of application: The MCU-PIT software serves to parameterize and commission the single-axispositioning control MCU 172A from the SIMODRIVE 611 family. It supports the simple programming and planning of data blocks. The software furthermore assists you during commissioning and servicing. MCU-PIT comprises two mutually complementary applications: PIT-EDIT and PIT-CONTROL. The MCU-PIT software also includes an online help system in the form of a paperless documentation SYSDOK-MCU. Product info: MCU-PIT: http://support.automation.siemens.com/WW/view/en/28305389 Hope this helps, Daniel Chartier |
Last edited by: O_Moderator at: 11/19/2010 8:51 AMlinks edited Last edited by: dchartier at: 11/18/2010 9:29 PM |
|
Follow us on