4/28/2013 1:43 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, In the manual release 2006/06 I have read: Working with a terminal program To be able to control the device directly via AT commands, use a terminal program, e.g. HyperTerminal. Note the following settings: Make the connection: COM port to which the device is connected Speed: 19200 Bit/s Data bits: 8 Parity: No Stop bits: 1 Duplex: Full Full is about the Duplex mode and not the control signals. In the same manual, the pinout is as follows: Signals (Signal direction DTE)SUB-D9 socket, Pin assignment RS232Pin1 DCD Output Pin2 RXD Output Pin3 TXD Input Pin4 DTR Input Pin5 GND Signal ground Pin6 DSR Output Pin7 RTS Input Pin8 CTS Output Pin9 RI Output A standard modem cable should fit. Have alos a look to this entry: Wireless Signaling and Switching via SMS with S7-300/400/ET200S Controllers and the MD720-3 GPRS/GSM Modem http://support.automation.siemens.com/WW/view/en/25545680 |
Last edited by: jklm at: 4/28/2013 1:50 PMBest regards |
|
4/28/2013 2:42 PM | |
Joined: 11/12/2008 Last visit: 4/20/2025 Posts: 221 Rating:
|
Hi, pin configuration for suitable cable is pin to pin connection. for AT see attached. Attachment25545680_Application_SMS_MD720-3_DOKU_V2_1_en.pdf (75 Downloads) |
HASSAN.S POJAILA |
|
Follow us on