12/20/2022 7:56 AM | |
Joined: 7/21/2021 Last visit: 9/14/2023 Posts: 14 Rating: (0) |
Hi Experts, Any answers ... |
12/20/2022 9:48 AM | |
Joined: 10/11/2006 Last visit: 7/26/2024 Posts: 5880 Rating: (799)
|
Hello OOP in Simotion is based on IEC61131-3 you are using the source-code (example-code) which described in capture 4.5.7.2 example ValveControl43 mit Error Reportingfor each chapter exists the corresponding example code in the book "OOP with simotion". prefere Capature 4.5.5. Interfaces as reference to classes Object-Oriented ProgrammingwithSIMOTION. Michael Braun. Publicis MCD. ,Book ISBN: 9783895784569
|
With best regards, |
|
This contribution was helpful to1 thankful Users |
1/11/2023 8:53 AM | |
Joined: 7/21/2021 Last visit: 9/14/2023 Posts: 14 Rating: (0) |
Hello JackD, Thanks for your answer.. |
Follow us on