8/17/2018 8:29 PM | |
Posts: 10 Rating: (0) |
[snip] However, I tried measuring a slot with a multi-meter. I expected when the slot was active, that I would see a spike in voltage, but I did not. I measured with the positive probe in the slot and the negative probe at ground. Shouldn't I see 24 V whenever the slot is active? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/20/2018 10:26:02 AMNew subject after splitting. Division of questions into separate topics. |
|
8/20/2018 8:17 PM | |
Joined: 7/7/2010 Last visit: 8/30/2024 Posts: 15125 Rating: (2412) |
Have you compared your wiring to the reference drawing for that module? https://support.industry.siemens.com/cs/mdm/83501523 then open the wiring -> wiring & block diagram section. Note it has 2L+, 3L+, 1M, 2M, 3M
|
science guy |
|
Follow us on