3/11/2021 8:38 AM | |
Joined: 12/18/2014 Last visit: 9/30/2024 Posts: 33855 Rating: (4210)
|
Is it a standing or a lying tank? |
3/11/2021 10:02 AM | |
Joined: 5/28/2018 Last visit: 9/25/2024 Posts: 29 Rating: (0) |
Is it a standing tank |
3/11/2021 1:32 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
Ech tank has a surface of 50 dm2, so every 2 mm of hihgt of level is 1 kg. Max 800mm = 400 kg Your sensor is 16000 Pa = 1,6 meter, thats 2x the tank, so 4-20mA = 0 - 800 kg. In mathematical blocks you can added every level. See attachment Attachment5 alaloog-totaal.zip (375 Downloads) |
3/11/2021 7:03 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
Its written in LOGO Soft version 8.3. Here is a lower version, try it, it work with Logo Soft Version 8.2 Attachment5xanaloog-0BA8.zip (359 Downloads) |
Follow us on