Industry Online Support
Technical Forum
1/5/2012 12:11 PM | |
Posts: 21 Rating: (0) |
Dear Friends, 6ED1056-5CA00-0BA0 (0BA4 Series) type memory card support this type 6ED1052-1HB00-0BA6 (0BA6 Series) LOGO CPU. With Regards, Venkatesh. S |
1/5/2012 12:17 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Which LOGO! memory/battery cards can be used with which LOGO! device series? |
1/5/2012 12:24 PM | |
Posts: 21 Rating: (0) |
Dear UMENCHO, i was mentioned the MLFB number na...... With Regards, Venkatesh. S |
1/5/2012 12:35 PM | |
Posts: 495 Rating: (58) |
My info is that this memory module could be only read by a LOGO! ...0BA6. Was this your question? Regards, |
1/5/2012 12:51 PM | |
Posts: 21 Rating: (0) |
Dear Mr. Mc Muffin, I want both read and write of the program. With Regards, Venkatesh. S |
1/5/2012 1:08 PM | |
Posts: 495 Rating: (58) |
Then you need this 6ED1056-1DA00-0BA0 LOGO! MEMORY CARD Regards, |
Follow us on