1/5/2022 1:48 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (9) |
For the memory card, it is clear to me. For the USB stick, the documentation of the pro panel states : 6AV6881-0AS42-...., which is a type that is not available anymore (the manual is from 2018). The manual of the normal comfort panel states : 6AV2181-8AS20-..... The only type refering to the last typenumber I can find back is : 6AV6881-0AS42-0AA1, which is a 32 GB Usb stick. Can this last type be used for the normal comfort panel and the comfort panel pro? Or are there other usb types suitable? |
1/5/2022 1:55 PM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168)
|
Hello, Yes, you can use 32 Gb USB stick, see technical information: https://support.industry.siemens.com/cs/nl/nl/pv/6AV6881-0AS42-0AA1/pi?dl=nl Best regards, Wizard |
1/5/2022 2:23 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (9) |
I suppose besides the memory size, there are no disadvantages for one or the other, when they are used for logging trenddata from the panel. The memory card, usb-stick will not or seldom be retracted from the device. I suppose both are as reliable concerning to data loss or corruption? |
1/5/2022 2:43 PM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168)
|
Hello, That is the right conclusion Best regards, Wizard |
Follow us on