11/5/2016 6:26 PM | |
Posts: 113 Rating: (1) |
Hi everyone What does mean this message and can I confirm it without a risk? |
11/5/2016 6:27 PM | |
Posts: 113 Rating: (1) |
When I confirm I have this message |
11/5/2016 6:48 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Here an overview of the memory concepts: |
11/5/2016 7:21 PM | |
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello,
Compressing blocks When data are compressed, gaps which have developed between memory objects in load memory/RAM as a result of load/delete operations will be eliminated. This releases free memory in a continuous block. Data compression is possible when the CPU is in RUN or in STOP. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on