4/30/2016 3:15 PM | |
Posts: 1 Rating: (0) |
Hello, I have the same problem with MICROMASTER Integrated MI400/3 9621-1DD60ZC92M88 (data from nameplate label) DriveMon detect COMBIMASTER2 without Version. When try to Open - there is "no drive selected" . When I make "new parameter set with factory setting" there is no offer for my device. If I pick out MICROMASTER, and option - Online (write RAM) there is a message: Configured device is COMBIMASTER version 3.0 and Identified device is COMBIMASTER2 version 93.0 After option Generate database, there is infinitely reading parameters and after few tens of thousands parameter, DriveMonitor stop responding and quit. Does anybody have some solution for me? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/2/2016 4:11:50 PMNew subject after splitting |
|
4/30/2016 4:04 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
SIMOVIS 6SE3290-0XX87-8SA2 software is required for this drive. |
Follow us on