Industry Online Support
Technical Forum
3/2/2011 11:13 PM | |
Joined: 6/4/2008 Last visit: 10/10/2024 Posts: 1502 Rating: (325)
|
Hi, as per the attached Midi Eco manual, it does not appear to be possible (unbelievably) to do this with parameters and Digital inputs. You can't even set a negative Fixed frequency as they appear to be clamped between 0 and 150Hz. I am assuming that you can't set P51 - P56 to a 2 (On Left) or a 3 (Reverse) as you could with the older Midimasters??? Regards, Graeme
AttachmentMME OperatingInst B.pdf (161 Downloads) |
Follow us on