8/30/2022 7:39 AM | |
Joined: 5/30/2022 Last visit: 5/30/2024 Posts: 524 Rating: (86) |
Hi ahuaranga, My recommendation is to install it on the PC, as this way you will use all the power of your PC, but before that I recommend you to check the compatibility of your version of Windows 10 with the version of TIA PORTAL that you are going to install, I attach the official compatibility Excel. NOTE: you can check the exact version of Windows with the winver command in the Windows search bar. AttachmentMicrosoft-Windows-10_en_2022-08-23.xlsx (162 Downloads) |
If this information really helps, you could use the Rate function. |
|
Follow us on