7/16/2013 7:17 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Ordering data are thereSTEP_7_V12_Orderlist I meant
Use Step7 5.x and those options It's possible to save other files on the MMC: http://support.automation.siemens.com/WW/view/en/15399111 And the complete programm, including Symbols and Comments: http://support.automation.siemens.com/WW/view/en/14053219 Personally I don't suggest you to go with TIA yet. Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 7/16/2013 7:19 PM |
|
This contribution was helpful to1 thankful Users |
7/16/2013 7:29 PM | |
Joined: 9/16/2011 Last visit: 9/10/2022 Posts: 291 Rating: (6) |
Use Step7 5.x and those options It's possible to save other files on the MMC: http://support.automation.siemens.com/WW/view/en/15399111 And the complete programm, including Symbols and Comments: http://support.automation.siemens.com/WW/view/en/14053219 Personally I don't suggest you to go with TIA yet. Best regards, Hristo Mihalev Why should not I go for TIA , is there any bug ? |
Reg, |
|
2/7/2018 2:51 PM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7957 Rating: (162) |
New question published by Dharala is split to a separate thread with the subject How can upload the PLC program in TIA V13 that was designed in TIA PORTAL V11?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on