7/8/2024 2:33 PM | |
Joined: 5/30/2022 Last visit: 7/9/2024 Posts: 551 Rating:
|
Hi, Depending on the environment in which the OP7 is programmed, whether protool or wincc flexible, you will have to make several jumps to migrate to TIA portal with a KP400: SIMATIC HMI HMI devices Comfort Panels Migration Guide At the CPU level, you would not have to change anything, since you can continue to communicate the KP with the S7-300.
|
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to
1 thankful Users |
Follow us on