5/19/2016 1:37 PM | |
Joined: 7/31/2014 Last visit: 1/29/2024 Posts: 11 Rating: (0) |
Hello friends, i have an issue.i am trying to migrate a project from Simatic manager to TIA v13. when i give the path of that project. my TIA shows following below errors (after exporting). The classic project is not consistent. "S7 Program(1)" needs to be recompiled.,5/19/2016,16:53:25 FC5: The interface of DB1 is out of date.,5/19/2016,16:53:25 Error during migration.,5/19/2016,16:53:25 Error during migration.,5/19/2016,16:53:25 i allready did the compilation of the project. still the problem is same.please guide me with your helpful comments. Snapshot of error is also attached below thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/19/2016 4:24:06 PMNew subject after splitting |
|
5/20/2016 7:52 AM | |
Joined: 7/31/2014 Last visit: 1/29/2024 Posts: 11 Rating: (0) |
hello ChristophD, ok. i got it. thanks for support. :) Thanks |
6/15/2016 12:16 PM | |
Joined: 8/21/2014 Last visit: 5/24/2024 Posts: 959 Rating: (13) |
New question published by vahid abdi is split to a separate thread with the subject Migration problems from STEP 7 V5.5 to TIA Portal. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on