2/20/2010 5:49 PM | |
Joined: 6/4/2008 Last visit: 3/20/2023 Posts: 1419 Rating:
|
Thanks Hristo, I would have thought so too, however, I'm following thisprocedure to migrate the HMI embedded in a Simotion project from Protool to WinCC, and when I reach step 6 after clicking the Step7 integrated icon, the project is selected, but there are no files shown which I can then open into WinCC Flex. Regards, Graeme
|
2/22/2010 4:27 PM | |
Joined: 5/12/2006 Last visit: 3/20/2023 Posts: 21352 Rating:
|
Hello, here the steps i have done for Migration from ProTool to WinCC. I used Simatic Step7 V5.4 SP5 and WinCCflex 2008 SP1 HF1. You must install WinCCflex in Fullmode so the Migration Wizard wil be installed on your system. Regards Christoph AttachmentHMI Migration.zip (106 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on