1/18/2023 10:07 AM | |
Joined: 10/1/2018 Last visit: 8/23/2024 Posts: 74 Rating: (1) |
Hello all, I would like to check an HMI screen visualization, which was programmed many years ago with the software Protool. But, since this software is obsolete and does not work in Windows 10, I need to convert it to WinCC flexible. The problem is that I tried to migrate it by opening the file .PDB, according to migration manual, but my WinCC does not have the option of opening Protool projects. Can anyone tell me how can I migrate to WinCC so I am able to open this visualization? Find attached the program I am trying to migrate to WinCC. Thank you in advance Best regards AttachmentTC731_NEVADO_2xTP170B_IBN_07_07_08.zip (782 Downloads) |
1/18/2023 10:46 AM | |
Joined: 8/6/2018 Last visit: 10/18/2024 Posts: 292 Rating: (40) |
Hello, The steps for the migration are the next: 1- Migrate to WinCC Flexible 2008 SP3/SP5. 2-Migrate to TIA. If project its in WinCC Flexible 2008 SP3 you can migrate to V13 SP1/SP2 or V14 SP1. If project its in WinCC Flexible 2008 SP5 you must migrate to V14 SP1 Upd 2 (or a newer update). You can't migrate directly to a newer TIA version because WinCC Flexible panels are not supported in TIA since V15 3- Change the panel to TP1200 Comfort. 4- Open project with V15/V16. Maybe this manuals or FAQs will help you: SIMATIC HMI WinCC flexible 2008 8 Migration https://support.industry.siemens.com/cs/ww/en/view/18796902 Migration of a WinCC flexible project integrated in STEP 7 V5.x to WinCC (TIA Portal) and upgrading of the operator panel version after a change of the WinCC (TIA Portal) version to a newer version. https://support.industry.siemens.com/cs/ww/en/view/77430539 Migration Tool TIA Portal https://support.industry.siemens.com/cs/ww/en/view/58638200 Thanks you |
1/20/2023 2:13 PM | |
Joined: 8/3/2009 Last visit: 10/18/2024 Posts: 13982 Rating: (1760)
|
Hello ismaelillo To migrate a Protool Projekt to WinCC flexible you need the Version WinCC flexible 2008 Sp2 or older. (its not possible With SP3/SP5) -> so you cannot use a Win10 system for that (use an older system or a VM Ware) -> you can download the installation files for 2008 Sp2 here: https://support.industry.siemens.com/cs/ww/en/view/100777999 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on