Industry Online Support
Technical Forum
6/24/2006 5:10 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi laid, FIRST OFF ALL: DON'T OPEN ON A NEXT QUESTION ON THE SAME THREAD A NEW THREAD!! PLEASE USE THE <REPLY> BUTTON ON THE BOTTOM OF A ANSWER SOMEBODY ELSE HAVE GIVEN!! [:P] The 6ES7335-7HG01-0AB0SM 335 - High-Speed Analog Input/Output Module for the S7-300 can read1 channel in 200 microseconds, all channels in 1mS. [:o] See http://support.automation.siemens.com/WW/view/en/1398483for the handbook. So you can choose for this card or the ET200S PN AI Card 6ES7134-4LB02-0AB0 which i have recomended 2 threads ago........ [:blush:] New ET 200S High Feature Analog Modules with 0.5ms Cycle Time Released for Delivery http://support.automation.siemens.com/WW/view/en/23417515when used in a ET200S HF PN then you can with the CPU315-2PN/DP or the CPU317-2PN/DP a fast communication. [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on