2/22/2015 9:42 AM | |
Joined: 5/12/2006 Last visit: 8/30/2024 Posts: 22348 Rating:
|
Hello, The Migration Tool is never installed with the TIA Portal!
For TIA V13 SP1/ SIMOTION V4.4.0.5 you must generate new migartion Files thats correct. Regards Christoph |
2/22/2015 10:09 AM | |
Joined: 1/4/2013 Last visit: 8/31/2024 Posts: 1119 Rating:
|
Thanks Christoph, but I solved this in another way : I found the Migration Tool V13 SP1 in a folder of the uncompressed files of the TIA V13 SP1, I double clicked and installed it. Then I was able to do everything. But I think that the main point is this :
You install the TIA V13 SP1 and you expect that the Mig tool is upgraded automatically from V13 SP0 to V13 SP1, but this doesn't happen. You have manually to browse the directories of the SP1 and search it (and also there are other interesting applications which I don't know...)... Anyway problem solved. |
Searching for Siemens used/new equipments ? |
|
Follow us on