6/20/2016 4:15 PM | |
Joined: 3/7/2016 Last visit: 4/14/2022 Posts: 7 Rating: (0) |
During openning project i am facing error message, please attach photo. Should i required to purchase this HSP missing software. or it is just kind of update?? please if possbile also share link to upload it. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/20/2016 5:33:44 PMNew subject after splitting |
|
6/20/2016 4:25 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello, Should be this: Updates for STEP 7 V13 SP1 and WinCC V13 SP1 - Siemens Industry ... |
This contribution was helpful to1 thankful Users |
6/20/2016 5:01 PM | |
Posts: 5225 Rating: (1192)
|
Hi there. Could you please tell us which software do you have? Do you know which devices are used in the program you are trying to open - PLC / HMI. It might simply just be an update of the hardware catelog you require. We are currently at TIA Portal V13 SP1 Update 8. If you have the "SIMATIC ET 200pro FC-2 SIMATIC ET 200pro FC-2 converter" in the project - than it is very likely you need the newest definition of the hardware. w |
Last edited by: William_B at: 6/20/2016 5:06:37 PMexpand answer |
|
6/21/2016 6:43 AM | |
Joined: 5/12/2006 Last visit: 8/8/2024 Posts: 22338 Rating: (3001)
|
Hello, this message is from STARTDRIVE. You open a projekt with devices which have Version V4.7 SP6. For this devices you need Startdrive V13 SP1 UPD3 + HSP. The files for Startdrive and the HSP you can found here: https://support.industry.siemens.com/cs/ww/en/view/68034568 Regards Christoph |
Follow us on