Industry Online Support
Technical Forum
5/26/2008 8:36 AM | |
Joined: 9/27/2006 Last visit: 7/13/2024 Posts: 12268 Rating:
|
Hello Praveen; The part number you are quoting is a singlepurchase number bor a Y-Link bundle, that includes the IM 153-2s, the Y-coupler and the bus modules required. But in the H-configuration you call directly the part number that is written on the IM 153-2s that are part of the bundle. Here is a short description of the steps to include a Y-link in the H-system configuration (from the Bus links DP/PA coupler, DP/PA link and Y-Link manual: http://support.automation.siemens.com/WW/view/en/1142696)Configuring Y linkThe Y link is configured in STEP 71. Start STEP 7 and in HW Config open your SIMATIC H station. 2. Drag an IM 153-2 (6ES7153-2Bxx1-0XB0) out of the PROFIBUS-DP\DP/PA directory from the hardware catalog to the redundant DP master system of an S7-400H. Result: The Properties dialog for the PROFIBUS interface of the IM 153-2 is displayed. 3. If necessary, change the proposed address of the IM 153-2 in the higher level DP master system. Result: After closing this dialog a dialog is displayed in which you can select the underlying master system. 4. Select PROFIBUS DP and confirm with OK.Result: The Y link is inserted into the redundant DP system. The default transmission speed of the underlying DP master system is 1.5 Mbaud. 5. If you want to change the transmission speed of the underlying DP master system, double-click on it. Result: The dialog with the properties for the underlying master system is displayed. – Select the "Properties..." button.Result: The "Properties PROFIBUS" dialog is displayed. – In the "Network settings" tab select a transmission rate ranging from 45.45 kBaud to 12 MBaud and confirm with OK. Of course, for the rest of the setup procedure, download and study the above manual. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/26/2008 8:38 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on