12/15/2008 7:30 AM | |
Joined: 10/3/2008 Last visit: 5/22/2024 Posts: 957 Rating: (123) |
Hi Safety1, do you know whether Q series supports the modbus protocol? If yes, then you could use"OpenModbusTCP PN CPU". Wüstenräuber |
12/15/2008 2:58 PM | |
Posts: 73 Rating: (20) |
Hello Wustenrauber, Thanks for the response. Yes they support Modobus TCP butthey must use a specialEthernet module to do Modbus TCP. Therefore extra cost. |
12/19/2008 11:46 PM | |
Posts: 5822 Rating: (411)
|
Hello, I think, if the Processor used on customer side fully supports the RFC 793 that the communication should work... on the S7 you need to use the T-Communication blocks, please check the manual |
This contribution was helpful to2 thankful Users |
Follow us on