Industry Online Support
Technical Forum
2/9/2010 12:30 PM | |
Joined: 6/3/2009 Last visit: 2/8/2024 Posts: 101 Rating: (7) |
Dear greenengineer How you are going to communicate with PC and Drive. |
2/9/2010 12:49 PM | |
Posts: 30 Rating: (2) |
Dont know could do with been able to plug a laptop into drive somehow do tests and gather date on laptop then unplug?? Many thanks |
2/10/2010 9:45 AM | |
Joined: 6/3/2009 Last visit: 2/8/2024 Posts: 101 Rating: (7) |
Dear greenengineer You can see the datalike speed (rpm), torque (Nm),power (kw) using DriveMonitor software. DriveMonitor software is to commissioning the Drive(Siemens). |
2/11/2010 5:38 AM | |
Joined: 6/3/2009 Last visit: 2/8/2024 Posts: 101 Rating: (7) |
Dear greenengineer YES can get from web site also. |
2/11/2010 7:46 AM | |
Posts: 378 Rating: (47) |
And if you want to know where, here it is http://support.automation.siemens.com/WW/view/en/11769381 best regards bilao |
2/17/2010 10:21 AM | |
Posts: 30 Rating: (2) |
Could someone help??....Can I get the Nm readout to display on a BOP ? If so how ??.................Many thanks simon |
Follow us on