5/7/2020 1:05 PM | |
Joined: 3/27/2008 Last visit: 5/10/2024 Posts: 1104 Rating: (138) |
Reference: MICROMASTER 440 Parameter List. https://cache.industry.siemens.com/dl/files/204/23708204/att_60463/v1/440_PLi_23708204_en_0106.pdf I have attached the drawing for the analogue input, this may help but I believe it does not go far enough. The 'Parameter List', link above; here some drawings, page 259, indicate the path of the analogue input, but tricky to follow the connections. I would reset the drive back to default and start again, however not knowing the complexity of the machine setup that is easy for me to say. It is working now, so you may opt to leave it, but something has been changed. It is unlikely that the drive has done this. I will leave this to you to think about, but please come back if i can offer any further help. (Looking at P0719, the default value is 0 in the manual?) Tractor AttachmentSiemens Micromaster 440 Parameter List.pdf (785 Downloads) |
Last edited by: Tractor at: 05/07/2020 14:17:01Tractor |
|
10/8/2021 12:31 PM | |
Posts: 2 Rating: (0) |
This post and conversation helped in trouble shooting drive problem of MM440. Thanks Tarun |
This contribution was helpful to1 thankful Users |
10/9/2021 10:44 AM | |
Joined: 3/27/2008 Last visit: 5/10/2024 Posts: 1104 Rating: (138) |
Thankyou for the feedback Tractor |
Tractor |
|
Follow us on