7/11/2014 12:58 PM | |
Posts: 1058 Rating: (93) |
See documentation of Parameterlist here (alarms and failures are also described there): parameter list MM440 In case you need the manual of MM440, you find it here. Select your language at bottom of page and then download the PDFs. regards |
7/12/2014 6:23 AM | |
Posts: 9 Rating: (0) |
i have enter all the parameters correct and dip switches are also in correct position,stilldrive is reading incorrect millliamps. |
7/14/2014 9:16 AM | |
Posts: 9 Rating: (0) |
sir,multimeter is not showing exact 4 milliamps it is showing 3.86-3.90 mA around and drive reading 0.57mA as i have mentioned earlier. |
Follow us on