Industry Online Support
Technical Forum
3/14/2013 6:26 PM | |
Posts: 13 Rating: (0) |
To back up parameters of a MM440 you have 3 ways: Through the softwares ( DriveMonitor, STARTER ) or throught a AOP (Advanced Operator Panel).
|
3/17/2013 7:54 AM | |
Joined: 3/21/2006 Last visit: 10/4/2024 Posts: 10229 Rating: (1181) |
Hello, Using profibus module of MM440 - Step7 plus DriveES software. http://support.automation.siemens.com/WW/view/en/30563626 Or directly DriveMonitor/Starter - http://support.automation.siemens.com/WW/view/en/6313369 Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
Follow us on