1/12/2024 4:18 PM | |
Joined: 4/15/2022 Last visit: 6/26/2024 Posts: 4 Rating: (0) |
Hello all of you! My Mobile Panel 177-DP gets a Error Message "Could not establish connection!" when im trying to connect it to PG for commissioning. The goal is to transfer a project on to the MP177DP. I checked the link: How can you transfer a WinCC flexible project serially to a panel? - ID: 23787153 - Industry Support Siemens - There was no new information for me. Im using PPI 6ES7901-3CB30-0XA0, since my computer does not have a serial-port im also using it with a serial to usb adapter to connect to my PC usb port. - Yes, i have installed driver for it and the COM-port config. is set to COM1 when connecting, RS232 communication thru COM1 is set on with deafult (Baudrate, Stopbit etc.) Im i using the wrong PPI cable, E-stand: 03 ? Kbaud rate is set to 19.2, Although it should not matter, freeport (dip-switch 5) on PPI cable is set to 0. I´ve tried et PG/PC to : S7 online(STEP7) --> PC adapter.PPI.1 i also tried: S7 online(STEP7) --> Serial cable.PPI.1. MP 177 DP in Transfer mode with only one channel enabled " Serial: via PPI RS232/PPI Multi-Master Cable " I have also tried with MPI/DP to USB cable without success. Would be overjoyed of some response. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/15/2024 09:39:37Link optimized. Last edited by: Jen_Moderator at: 06/06/2024 06:51:50New subject after splitting Last edited by: sinuswavesurfer at: 06/06/2024 19:45:38Last edited by: sinuswavesurfer at: 06/06/2024 19:54:50May the waves be with you |
|
Follow us on