Industry Online Support
Technical Forum
6/15/2009 1:06 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Adham,
Perhaps manual could be helps: Entry-ID 1220184 Regards Hristo Mihalev |
6/15/2009 2:56 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating: (94) |
Are you getting any errors for your modbus block calls (FB7 and FB8)? Also, first try the sample program that gets installed with the Modbus PTP drivers. Try using a simulation software (likeModsim) to simulate your slave and see if you can get it to work. |
6/15/2009 3:07 PM | |
Joined: 2/6/2009 Last visit: 6/18/2024 Posts: 939 Rating: (118) |
Hi, I have faced the same problem once. My all settingswas ok. Finally I found that the "Modbus receive Block" FB7 was not called (enabled).Check the receive blockcall (Check in online). Please try to use the "CPUCLock Memory Byte" (1 sec pulse) togive the REQto the "Modbus Send Block" FB8 for testing purpose. The main thing is you have to give( 'X') this symbol at the "R_typ" of "Modbus Send Block" FB8 otherwise it wont work. Please find the attachment for the example of Modbus Block calls. Try the above options, if not working means let me know. AttachmentModbus Blocks Call.pdf (134 Downloads) |
_______________________________________________________________ |
|
Follow us on