1/27/2018 12:46 PM | |
Joined: 5/28/2014 Last visit: 12/31/2023 Posts: 32 Rating: (0) |
I have S7-1500 CPU with ET200SP Interface Module and my CM PTP card is an ET200SP type.It is a Modbus Master configuration. I am simulating my program with Modbus Slave Simulator. I am using two-wired protocol RS485 and I have also moved 4 in the Modbus_Comm_Load variable Mode. I am using TIA Portal v14. In Modbus_Comm-Load I have a status 7000 and in Modbus_Master I have 7001 and 7002. I have Tx flashing but no Rx. My slave ID is 2. Backup and Screenshots are attached. AttachmentET200SP Modbus.zip (200 Downloads) |
Follow us on