2/1/2013 1:58 PM | |
Posts: 3093 Rating: (323)
|
Hello Manmeet, are the two CP343-1 located in the same rack? If yes, you can use ModbusTCP RED V2. Regards, Kaulquappe |
2/1/2013 2:13 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Kaulquappe, Thanks for quick reply ! Both CP are in same rack. Good to know that it can be done. Butthislink does not talk about redundant CP 343-1. ModbusTCP RED V2, is this the one with part number2XV9450-1MB11? Regards, Manmeet.
|
7/14/2017 1:14 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by Tan Bui is split to a separate thread with the subject Can use two CP for redundancy connect to Master (CPUA or B) via two different HUBs, and with different subnet . Best regards |
Follow us on